Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Thermal Unit Selection Tables for Pre-Type S NEMA Starters
Issue:
Customer is looking for the amperage for an A.39 and A.47 for a pre type S 8536AO starter

Product Line:
NEMA Pre Type S Starters

Environment:
NEMA Contactors and Starters

Resolution:
The customer will need to check on the thermal unit tables that came with the starter itself.
These devices went obsolete in the Mid-1960s, but thermal units are still available.