Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a 400A - 600A GS2 Disconnect switch use a 9422 Handle?
Issue:
Can I use 9422A1 handle with GS2SU3?

Product Line:
Operating Mechanism and Disconnect Switches

Environment:
GS2 Disconect Switches

Resolution:
No, since that the cable operator kits for GS2 switches can only go up to 200A

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings