Issue:
Is a 400V BA9s light module with NO and NC contacts can be used with 22mm emergency stop operators?
Product Line:
Push buttons and operator Interface
Environment:
XB4, ZB4, XB5, ZB5
Answer:
There are no illuminated E-stop mushroom heads that would work with BA9s light module. The ZB4BW643 or ZB5AT8643M push/pull and ZB5AW743 turn to release mushroom head push button can only be used with protected LED light modules. The LED light module is only available from 12Vac/dc up to 240Vac.
Is a 400V BA9s light module with NO and NC contacts can be used with 22mm emergency stop operators?
Product Line:
Push buttons and operator Interface
Environment:
XB4, ZB4, XB5, ZB5
Answer:
There are no illuminated E-stop mushroom heads that would work with BA9s light module. The ZB4BW643 or ZB5AT8643M push/pull and ZB5AW743 turn to release mushroom head push button can only be used with protected LED light modules. The LED light module is only available from 12Vac/dc up to 240Vac.
Released for: Schneider Electric Canada