Issue:
Can the ERMS feature be used on breakers installed in P1200 style enclosures?
Product Line:
ERMS (Energy Reduction Maintenance Switch)
Resolution:
The ERMS solution is available on breakers mounted in the P1200 enclosures, HOWEVER, the ERMS parts (the switch, I/O module, etc.) CANNOT be mounted in the enclosure with the breaker. They would have to have their own separate enclosure.
Can the ERMS feature be used on breakers installed in P1200 style enclosures?
Product Line:
ERMS (Energy Reduction Maintenance Switch)
Resolution:
The ERMS solution is available on breakers mounted in the P1200 enclosures, HOWEVER, the ERMS parts (the switch, I/O module, etc.) CANNOT be mounted in the enclosure with the breaker. They would have to have their own separate enclosure.
Released for: Schneider Electric Canada