Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the demand interval range for the PM8000?
Issue
What is the demand interval range for the PM8000

Product Line
PM8000 series meter
PM8240
PM8243
PM8244

Environment
ION Setup
User Guide, Meter Configuration, Settings and Characteristics

Cause
Need to know the range the demand sub-interval length can be set to in the PM8000 series meter.

Resolution
The demand sub-interval length value must be between 1 second and 99 minutes.

To configure the meter's Demand interval using ION Setup:
  1. Start ION Setup.
  2. Open the Setup Assistant for your meter.
  3. Navigate to Demand > Rolling Block.
  4. Configure the Sub-interval Length by selecting the parameter and clicking Edit.
  5. Once the parameter has been configured, click OK to save the setting to the meter.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings