Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the HJQLLC IP2X line cover work with the Q2 2 pole main breaker?
Issue:
Does the HJQLLC lug cover work with 2 pole main breakers?

Product Line:
Panelboards

Environment:
NQ Panelboards

Resolution:
No. 3 pole breakers only. However, they can use a 3 pole Q2 breaker and just wire the A and C phase only.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings