Issue:
Instruction bulletin for the 8502SA* and 8536SA* breakdown
Product Line:
NEMA Contactors and Starters
Environment:
Class 8502/8536 Contactors and Starters
Resolution:
The attached files are for SERIES B Starters Class 8502/8536, 2 and 3 poles, using the melting alloy or solid starter overload relay.
File name 30072-013-52 using the solid state overload relay
File name 30072-013-08 using the melting alloy overload relay
Instruction bulletin for the 8502SA* and 8536SA* breakdown
Product Line:
NEMA Contactors and Starters
Environment:
Class 8502/8536 Contactors and Starters
Resolution:
The attached files are for SERIES B Starters Class 8502/8536, 2 and 3 poles, using the melting alloy or solid starter overload relay.
File name 30072-013-52 using the solid state overload relay
File name 30072-013-08 using the melting alloy overload relay
Released for: Schneider Electric Canada