Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Looking for a shaft for a handle and switch. VLS3P100R2 switch and VLSH3S7RD (red) or VLSH3S7BD (black) handle.
Issue:
What is the 200 mm shaft used for VLS3P100R2 switch and VLSH3S7RD (red) or VLSH3S7BD (black)  handle?

Product Line:
Operating Mechanism and Disconnect Switches

Resolution:
Only available in VLSS1505 (150 mm)
and VLSS3005 (300 mm).

VLSS2005 (200 mm) is not recognized on Q2Cash Tool.

It was decided not to market the 200 mm shaft as the 300 mm can be cut down if needed.
Reference: 9400CT1601

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings