Issue
How can the minimum or maximum demand values be found on the PM8000 front panel?
Product Line
PM8000
Environment
Metering & Power Monitoring
Cause
Where to find the screen that contains the minimum or maximum demand values via the PM8000 front panel.
Resolution
From the meter front panel:
How can the minimum or maximum demand values be found on the PM8000 front panel?
Product Line
PM8000
Environment
Metering & Power Monitoring
Cause
Where to find the screen that contains the minimum or maximum demand values via the PM8000 front panel.
Resolution
From the meter front panel:
- Press ‘Home’ to display the menu
- Press ‘Up’ or ‘Down’ until Power is highlighting
- Press ‘Check mark’ to view the power screens
- Press ‘Down’ until Demand is highlighted
- Press the ‘Check mark’ to view the Demand screens
- Press the ‘+’ to show a list of additional screens for Total Demand Delivered or Press the ‘Down’ and then the ‘+” to show a list of the additional screens for Total Demand Received
- Choose the additional screen to view the minimum or maximum Total Demand Delivered/ Received values
Released for: Schneider Electric Canada