Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the ZBY9330 legendswork on the XALK yellow station with red mushroom head push button 40mm turn to release?
Issue:
What is the part number for the round Emergency Stop legend for XALK enclosures?

Product Line:
Harmony Control Stations

Environment:
Push Buttons and Operator Interface

Cause:
Product Features

Answer:
The circular Emergency Stop legends will not work on the XALK enclosures. There is a raised area on the front of these XALK enclosures which will not allow a legend to be mounted flush to the surface.

Schneider Electric Canada

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings