Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the Schneider Energy Monitor compatible with my home?

To ensure you have the best experience with your Schneider Energy Monitor, we recommend you meet the following compatibility specifications:

Your home has:

  • 2.4Ghz Wi-Fi network with consistent internet connection. The monitor is not compatible with 5Ghz Wi-Fi signals.
  • Its own electrical meter and accessible electrical panel.
  • Your mobile device runs on iOS or Android and has Bluetooth and Wi-Fi connectivity.

Your electrical panel:

  • Is a split-phase 120/240V panel OR split-phase 120/240V 400A split-service panels (each panel rated up to 200A) with a second set of sensors.
  • Must have enough space to fit sensor clamps with HxWxD dimensions of 3.375" x 2" x .75" (85.73 x 50.8 x 19.05mm), and an inside diameter of 1”. The current sensors may not be able to fit around busbars. Our sensor cables are 46" (116.84cm) long and our power cable is 36" (91.44cm) long.
  • Does not drop below 32°F (0°C) or exceed 154°F (68°C).
  • Is not exposed to water or areas with high condensation (Schneider complies with ANSI/IEC 60529 Rated IPx0).

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings