Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a special tool needed for installing 225A-600A I Line Busway, ie. AP504G10?
Issue:
Tools needed for installing 225A-600A I line Busway?

Product Line:
I line Busway

Environment:
Products sold in North America

Resolution:
No tools are needed to install. See the instruction bulletin, 45123-174-01.  The only tool needed is a screw driver to install the grounding screw on top of  the Busway.

Schneider Electric Canada

Attachment(s)
225 to 600A 45123-174-01D.pdf [917.93 KB]
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings