Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the ION8650 compatible to save waveform data in COMTRADE format?

Issue
Is the ION8650 compatible to save waveform data in COMTRADE format?

Product Line
ION8650

Environment
Waveform data (COMTRADE format)
ION Setup

Cause
Can the meter provide waveforms in COMTRADE format?

Resolution
Only the ION8650A meters can save waveform data in COMmon Format for TRAnsient Data Exchange (COMTRADE) format, which is then available for download via FTP. This is intended for use in conjunction with IEC 61850 and is only available on ION8650A meters with an Ethernet port.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings