Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What hardware is required for M580 backplane expansion?

Issue
Need to know the components required to expand an M580 backplane.

Product line
Modicon M580

Resolution
Adding an expansion rack requires an Extension rack Module (BMXXBE1000), Extension rack Cable and Terminators.
The BMXXBE2005 is an Extension rack kit that contains everything that you need including:

  • 2 BMXXBE1000 extension rack modules
  • one BMXXBC008K 0.8 meter extension cable
  • one TSXTLYEX set of 2 line terminators

Other cable lengths available:
BMXXBC015K - 1.5m extension rack cable.
BMXXBC030K - 3m extension rack cable.
BMXXBC050K - 5m extension rack cable
BMXXBC120K - 12m extension rack cable

*Any single item from the kit can also be ordered separately.


If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings