Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the plug-in mounting bases for the Powerpact L and the Compact NS630 interchangeable?
Issue:
Can the NSX630 breaker use the Powerpact L mounting base?

Product Line:
Circuit Breakers

Resolution:
These plug-in mounting bases are not interchangeable.
NSX and Powerpact use the same plug-in base AAV41536 (0099539001), but kits LV432516 and S32514 assemblies have a different configuration.
Therefore, the NSX and Powerpact mounting bases cannot be used for the other breaker.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings