Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why do I get a 'Module not allowed in this position' message when adding a Hart module?
Issue
When using Control Expert / Unity Pro to add either a BMEAHI0812 or BMEAHO0412 in an empty slot it is not allowed.

Product line
Modicon X80, Control Expert, Unity Pro

Resolution
When using the BMEXBP1002, slots 2 and 8 do not support BME******* Ethernet backplane IO modules. Slots 2 and 8 only support BMX******* XBUS backplane IO modules. All of the remaining slots support either BME or BMX modules.

This also applies to the BMEXBP1200 for slots 2,8,10 and 11.



Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings