Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the replacement part number for the coil cover for Class 8502 or Class 8536 Type SF*?
Issue:
Is the coil cover for class 8502 or 8536 type SF replaceable?

Product line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 8502 or 8536 Contactors and Starters

Resolution:
31091-048-50, due to UL restrictions nameplate is not included.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings