Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many thermal units are required for a Class 2510 Type M 2 pole unit?
Issue:
Need to know the number of thermal units he needs for the 2510M/T manual starters.

Product Line:
Manual Starters and Switches

Environment:
Class 2510 Starters

Resolution:
Based on the fact that the current on single phase is the same in both legs, only 1 thermal unit is required for single-phase starters.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings