Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What does suffix 35 indicate on a circuit breaker?
Issue:
Meaning of suffix 35 on a circuit breaker.

Product Line:
Molded Case Circuit Breaker

Resolution:
Suffix 35 indicates that the breaker is factory calibrated for a 50°C ambient temperature instead of the standard 40°C. Breakers with suffix 35 are not UL listed.
This suffix does not apply to Multi-9, Powerpact, Masterpact breakers, or legacy breakers with Micrologic trip units.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings