Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a 9001K15 30mm Emergency Break Glass Operator a complete device?
Issue:
9001K15 assembly and parts

Product Line:
Type K Heavy Duty Specialty Operators

Environment:
30 mm Push Buttons

Resolution:
It includes everything except the contact blocks. Suggest using normally open early closing.

Replacement Parts:
DescriptionPart number
Yellow bumper 3105211101
Hammer and chain 3105206750
Lower ring nut 6512232801 (Obsolete)
Top ring nut 9001K40
Package of 5 replacement discs 9001K57
Clip to hold hammer 2540902240

Note: We do not offer a red bumper for these

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings