Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the minimum level of current displayed by Micrologic trip units on Powerpact M, P, and R frame and Masterpact breakers
Issue:
Inaccurate reading on the LCD Display of the Ammeter trip unit

Product Line:
Circuit breaker

Resolution:
With current flow between 0 and 20% of sensor value, the ammeter may not be accurate.
Even with external power supplied, current through the circuit breaker must exceed 0.20 x In for the ammeter reading to be accurate to within 1.5%.

> Below 0.1 x In, measurements are not significant
> Between 0.1 x In and 0.2 x In, accuracy changes linearly from 4% to 1.5%
> Between 0.2 x In and 1.2 x In, accuracy = 1.5%

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings