Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are there QO or QOB breakers with equipment protection ground fault?
Issue:
Equipment Protection Ground fault device

Product Line:
Miniature Circuit Breaker

Resolution:
Yes, there are 30 mA ground fault protection (EPD) breakers in 1 pole, 15-30 A with the following part numbers:

QO(B)115EPD
QO(B)120EPD
QO(B)125EPD
QO(B)130EPD

2-pole 15-60 A:

QO(B)215EPD
QO(B)220EPD
QO(B)225EPD
QO(B)230EPD
QO(B)240EPD
QO(B)250EPD
QO(B)260EPD (Only 240 Vac and 208 Vac two-wire loads. Does not contain load neutral connection)

3 pole, 15-50 A:

QO(B)315EPD
QO(B)320EPD
QO(B)330EPD
QO(B)340EPD
QO(B)350EPD

Square D also offers 100 mA ground fault protection (EPE) in 3 pole only:

QO(B)315EPE
QO(B)320EPE
QO(B)330EPE
QO(B)340EPE
QO(B)350EPE

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings