Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a NEMA 4X rated Mini Power Zone (MPZ) ?
Issue:
Are Stainless Steel MPZ's N4 or 4X rated?

Product Line:
LV Transformers

Environment:
MPZ

Cause:
Enclosure type

Resolution:
No, the Stainless Steel MPZ Mini Power Zone is not available in a NEMA 4X version.
The Stainless Steel enclosure NEMA rating is 3R and comes standard with #304 stainless steel. Square D does offer a painted #316 grade Stainless Steel enclosure as well but it is still only has a NEMA 3R rating.

Schneider Electric Canada
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Product Selectors
  • Software and Firmware
  • Product Substitution and Replacement
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings