Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the DT363, series F5? (may be shown as F05)
Issue:
DT363, series F5 field replaceable parts.

Product Line:
Safety Switch

Environment:
Double Throw Safety Switch

Cause:
Maintenance

Resolution:
The repair parts for the DT363, series F5 (F05) are as follows. No other parts are available.
-Line Base - 4056775150 (one each upper and lower; order arc suppressor and wire assembly separately)
-Line Base mounting screws - 4020515101 (requires 3 per line base)
-Load Base - 4056604650 (one each upper and lower; order lugs and wire assembly separately)
-Load Base mounting screws - 4020515101 (requires 2 per load base)
-Arc Suppressor Assembly - 4056635550 (requires 1 per line base; obsolete, no longer available, replaced by NNZ51874)
-Arc Suppressor mounting screw - 4020514501 (requires 1 per arc suppressor)
-Wire Assembly - 4056621050 (requires 1 per phase; includes cable factory connected mechanical lug at one end and at other end a crimped connector; use mounting screws of line and load lugs)
-Line and Load Lug Assembly - 4025101851 (per lug - line, load)
-Line, Load Lug mounting screw - 4020514202
-Ground Lug - 4025101851 (per lug)
-Ground Lug mounting screw - 4020514801
-Switch Mechanism - 4056646950 (each for upper and lower)
-Linkage Assembly - 4056614950 (links together upper and lower switch mechanisms)
-Linkage Assembly mounting screws - 2299940562 (requires 7)
-Handle - 4056688750
-Lockplate - 4056673301
-Lockplate mounting screws - 2299940562
-Cover Latch - 4056607201 (each for upper and lower; also requires cover latch spring)
-Cover Latch Spring - 4022304301 (each for upper and lower; also requires cover latch)

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings