Issue:
Identify the size of the run starters in 8606 reduced voltage starters
Product Line:
Class 8606 Reduced Voltage Starters
Environment:
Square D NEMA Contactors and Starters
Resolution:
It depends on the NEMA size of the RVAT. NEMA sizes 2 through 4 have the same size Start contactors as the Run starter. Size 5 RVAT uses size 4 Start contactors and a size 5 Run starter; size 6 RVAT uses size 5 Start contactors and a size 6 Run starter; etc.
Identify the size of the run starters in 8606 reduced voltage starters
Product Line:
Class 8606 Reduced Voltage Starters
Environment:
Square D NEMA Contactors and Starters
Resolution:
It depends on the NEMA size of the RVAT. NEMA sizes 2 through 4 have the same size Start contactors as the Run starter. Size 5 RVAT uses size 4 Start contactors and a size 5 Run starter; size 6 RVAT uses size 5 Start contactors and a size 6 Run starter; etc.
Released for: Schneider Electric Canada