Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the material of the NW molded case? And what is its fire or flame retardency rating?
Issue:
What is the case material for the NW breaker?  And what is its fire or flame retardency rating?

Product Line:
Molded Case Breaker

Environment:
Masterpact NW

Resolution:
The material of the NW case is MENZOLIT CIC 25630 grey 49-905/220
Fire endurance as HN60E02 and CEI695-2-1 standard.
.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings