Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What Class of fuse does ALL the 100amp General Duty Safety Switches use (for example, D223N, CH223N, D223NRB, CD223NRB, D323N, CD323N, CD323NRB and D323NRB)?

Article available in these languages: Spanish

Issue:
Product design features

Product Line:
General Duty Safety Switches

Environment:
Fuses

Cause:
Installation

Resolution:
NOTE: Schneider Electric DOES NOT Manufacture or Sell Fuses for General Duty Heavy Duty or Double Throw Safety Switches.

The 100amp General Duty Safety Switches accept Class H or K fuses as standard. For design Series F01 or F03, options include Class R fuses (field install Class R Fuse Kit RFK10). With Class H or K fuses installed, the switch is UL/CSA listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R fuses (and RFK10 fuse kit installed) the switch is UL/CSA listed for use on systems with up to 100,000 RMS Symmetrical Amperes available fault current.

NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings