Issue:
If I have an exisitng QMB364 switch , can I use the Series E1 QMB364W Switch?
Product Line:
QMB Panelboards.
Environment:
QMB Switches.
Cause:
Product Design Features
Resolution:
The QMB364 Series D2 , 200A switch , is a replacement for the QMB3620 Series 1-4 switch.
Due to the drastic QMB364 Series D2 design differences, a Current Series E1, or greater Series QMB364W switch, cannot be used in place of a Series D2 switch.
The QMB364W is electrically equivalent to the QMB364 and older QMB3620, but current Series E1 , and D2 are not interchangeable.
If I have an exisitng QMB364 switch , can I use the Series E1 QMB364W Switch?
Product Line:
QMB Panelboards.
Environment:
QMB Switches.
Cause:
Product Design Features
Resolution:
The QMB364 Series D2 , 200A switch , is a replacement for the QMB3620 Series 1-4 switch.
Due to the drastic QMB364 Series D2 design differences, a Current Series E1, or greater Series QMB364W switch, cannot be used in place of a Series D2 switch.
The QMB364W is electrically equivalent to the QMB364 and older QMB3620, but current Series E1 , and D2 are not interchangeable.
Released for: Schneider Electric Canada