Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Customer is trying to determine the complete number for XCKJ limit switch. <br />
Issue:
How to get XCKJ limit switch complete part number?

Product Line:
Limit Switches

Environment:
XCKJ Limit Switch

Resolution:
Look for numbers on body and head that begin with ``Z``. Take the number for body , which will begin ZCKJ, change the Z to an X than add the two numerical digits of operating head and the last two digits of lever arm if switch is lever arm actuated. (eg. body ZCKJ1, operating head ZCKE055 and lever arm ZCKY11 as a complete device would be XCKJ10511) It may not be advisable to order this as a completed assembly, depending on stock levels of components and lead times. Rather, order the components and assemble them in the field. This technique may also be used to work backward from a complete assembly to components.

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings