Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are welded base channels for panelboards only available in Nema 3R/12 applications?
Issue:
Are welded bas channels available for panelboards?

Product Line:
Panelboards

Environment:
UL 67; UL 50; CSA C22.2 No.'s 20-M1989 & 94-M91, 29 & 94-1989; NEMA PB1; NFPA 70 Art. 408; Federal Specification W-P-115C Type 1 Class 1 ; 2003 IBC; NFPA 5000; ASCE/SE17;2000 IBC, 1995 NBCC

Cause:
Welded base channels allow the normally wall-mounted enclosure to be free-standing.

Resolution:
Welded base channels are available for NF, NQ, I-Line and QMB panelboards with a Nema 1 rated enclosure.  For Nema 3R/12, we offer them only if the panelboard is to be mounted indoors.  In order to get welded Base channels they must be selected in product selectors as special Tag .