Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the 8539 combination starters in NEMA 7 & 9 bolted enclosures UL Listed?
Issue:
Is the 8539 combination starters line in NEMA 7 & 9 bolted enclosures UL Listed?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
NEMA combination starters

Resolution:
No, only the NEMA 7 & 9 devices in Spin Top enclosures are UL.

Revised 2011: Nema 7 and 9 explosion proof enclosures are no longer available for Nema starters/contactors.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings