Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What retaining kit is required for backfeeding a 2 pole branch circuit breaker in a Homeline load center, series S01, S02, S03, or S04?
Issue:
Retaining kit for Homeline load centers, series S01, S02, S03, or S04.

Product Line:
Load Centers

Resolution:
  • HOM1RK secures one 2 pole branch circuit breaker when used as a back-fed main for HOM612L100F, HOM612L100S, HOM612L100RB, HOM48L125GC, and HOM48L125GRB.
*** NOTE: HOM612L100F, S, or RB restricted to maximum 100 A back-fed main breaker. HOM48L125GC, RB restricted to maximum 125 A back-fed main.
*** NOTE: HOM612L100F, S, or RB is series 001 or 1
  • HOM4RK2LA secures one 2 pole, branch circuit breaker to the right side of the interior when used as a back-fed main for 125 A convertible main load centers, series S01, S02, S03, or S04.
*** NOTE: Restricted to maximum  125 A back-fed main breaker.
  • HOM4RK2HA secures one 2 pole, branch circuit breaker to the right side of the interior when used as a back-fed main for 150 - 225 A convertible main load centers, series S01, S02, S03, or S04.
***NOTE: Restricted to maximum 125 A back-fed main breaker.
  • HOM5RK secures one 2 pole, 150 - 200 A branch circuit breaker when used as a back-fed main for 150 - 225 A convertible main load centers, series S01, S02, S03, or S04.
***NOTE: The back-fed main breaker amperage cannot exceed the amperage rating of the load center.
***NOTE: The 150 - 200 A branch circuit breakers require 4 spaces to mount on the load center interior.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings