Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the rating plug need to be removed for hi-pot or dielectric testing on breakers with the P and H trip units?
Issue:
Does the rating plug need to be removed for hi-pot or dielectric testing on breakers with the P and H trip units?

Product Line:
Micrologic

Resolution:
Yes. But it is not necessary to remove the rating plug on the basic and A trip units.

Dielectric tests (high potential, insulation resistance, or Megger tests) may damage Micrologic® P and H trip units.
• Remove rating plug from trip unit prior to testing.
• Replace trip unit if rating plug was not removed during tests or if trip unit was exposed to more than 700 Vac.
Failure to follow these instructions can result in equipment damage.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings