Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between an STR23SE and a STR23SP?
The only real difference is in the instantaneous settings. The STR23SE has a maximum setting of 10 where the STR23SP has a maximum setting of 9. Note that the SP is for UL listed breakers, and the SE for IEC breakers.


CTA-ID : 2002861

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings