Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the available incandescent bulbs or lamps for XBV Lens?
Issue:
What is the replacement lamp for a XVBC4M flashing indicating bank?

Product Line:
Tower Lights and Beacons

Environment:
XVB - 70mm Diameter Beacons

Resolution:
This flashing unit XVBC4M uses a 10W incandescent lamp. It will accept a 48 to 230 volt AC supply.
Incandescent bulbs bayonet type BA 15d,10 watts12 Vac/dcDL1BLJ
24 Vac/dcDL1BLB
48 Vac/dcDL1BLE
120 Vac/dcDL1BLG
230 Vac/dcDL1BLM
Incandescent bulbs bayonet type BA 15d, 7 watts12 Vac/dcDL1BEJ
24 Vac/dcDL1BEB
48 Vac/dcDL1BEE
120 Vac/dcDL1BEG
230 Vac/dcDL1BEM

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings