Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the advantages of the Energy Center over a standard combination service entrance device (CSED)?
Issue:
What advantages does the Energy Center have over normal CSEDs?

Product Line:
Energy Center

Resolution:
Energy Center has multiple advantages over a standard CSED. It is designed to support backup power from various distributed energy resources (solar, battery, and generator) and can easily be converted from partial to whole home backup.
Energy Center comes with the following items factory installed:
• QO215 - 15 A, 2 pole circuit breaker (to protect Wiser Energy)
• (2)QO2110 - 110 A, 2 pole, submain circuit breakers (factory wired to the power distribution block)
• SQR44201WH - 20 A convenience outlet (factory wired to the GFI MCB)
• QO120PGFI - 20 A GFI miniature circuit breaker
• QO250PSPD - whole home surge protection device
• Wiser Energy monitoring kit
• (2) hold down brackets/screws (for the solar circuit breaker - sold separately)