Issue:
For standby generator with ATS, does the ATS wire into the power distribution block in the Energy Center?
Product Line:
Energy Center
Resolution:
If there is no battery backup system, the PDB can be used to wire an ATS to provide either whole house or partial house backup. If there is a battery backup system, then the isolation relay for that system will have used the PDB connections already. In that case, a standby generator will have to use the ATS and generator controls built into the backup interface for the battery backup system.
For standby generator with ATS, does the ATS wire into the power distribution block in the Energy Center?
Product Line:
Energy Center
Resolution:
If there is no battery backup system, the PDB can be used to wire an ATS to provide either whole house or partial house backup. If there is a battery backup system, then the isolation relay for that system will have used the PDB connections already. In that case, a standby generator will have to use the ATS and generator controls built into the backup interface for the battery backup system.
Released for: Schneider Electric Canada