Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
If the LED blinking pattern has stopped on an AF or AFGF breaker, can it be re-initiated to determine the last trip?
Issue:
How can the LED on the AF and AFGF breakers be re-initiated to determine the cause of the last trip?

Product Line:
QO and HOM arc fault and dual function breakers

Resolution:
There are two ways to re-initiate the LED blinking pattern:
1) Do a quick press and release of the test button (holding down will trip the breaker)
2) The LED will re-initiate its blinking pattern when the breaker is turned on