No, 15A receptacles only accept 14AWG solid copper wire in the push-in holes. It is best practice to use the side pressure plates which will accept the 12AWG straight wire and more securely capture the wire when the screws are tightened.
Do X Series Wiring Devices support copper-clad aluminum (CCA)?
Released for: Schneider Electric Canada