Issue:
Quantity of busbars that can be used inside the enclosure for interconnect GV2's
Product Line:
TeSys Deca Contactors
Environment:
Panel building
Resolution:
There is no really limit of busbars that can be used for the GV2. The maximum use of busbars Its based Between supply, heat generation, panel space, etc
The biggest limitation is actually around the max ampacity of contactor. The qty really depends on the application
so for example on 63 Ampacity if customer has a bunch of 10A devices. The max number of GV on bus would be 6 (6x10=60A)
any configuration for bus would work but that ampacity is the stopping point.
however, in the same situation, if there are a bunch of 2 AMP motors, theoretically you can have up to 31 with continuous
bus connections if the supply and the panel can handle that with heat dissipation and size.
Released for: Schneider Electric Canada