Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to solve Tesys T Fault code 60?
Issue:
I have a Tesys T with error code 60 "L2 current or voltage detected in single-phase mode", how to solve it?

Product line:
Tesys

Environment:
TeSys T Motor Management System

Resolution:
Single phase voltage is measured from L1 and L3
Use as example the following wiring diagram extracted from the installation guide.
The phases need to be wired to L1 and L3 (Not detecting voltage/current on L2)

Tesys T single phase wiring

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings