Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the class of fuse used for 8998KY410?

Issue:

What is the class fuse used for 8998KY410?

Product Line:

LV Motor Control Center

Environment:

Model 4 MCC

Resolution:

The standard bucket comes with Class H fuse clip , but can also use a class R fuse, order the HRK1020 class R fuse kit.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings