Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is temperature rating for the lugs used with NEMA contactors?
Issue:
Temperature rating for power lugs on NEMA contactors

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
8502 NEMA Contactors

Resolution:
They're sized for 60°C wire ampacity, rated for 60°C minimum or for 75°C wire ampacity, rated 75°C minimum.
* The power lugs are suitable for copper conductors only.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings