Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can a DTX file be restored in the simulator?

Issue
Looking to view the contents of a DTX file but do not have any hardware. Can the DTX file be restored in the Control Expert Simulator?

Product Line
Unity Pro, Control Expert, Modicon M580, Modicon M340, Modicon Momentum

Resolution
Yes. A DTX file can be restored in using the Simulator, but all of the same rules for using an actual PLC must be followed. This means that the simulator must be loaded with a project/PLC that is compatible with the DTX file.