Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What class of fuse do ALL the 30 A, 240 Vac max, heavy duty safety switches accept (for example, H321, CH321, H321RB, CH321RB, H321DS, CH321DS, H321AWK, and CH321AWK)?

Product Line:
Heavy Duty Safety Switches

Resolution:
HDSS = heavy duty safety switches
SCCR = short circuit current rating

All the 30 A, 240 Vac max, HDSS accept Class H or K fuses as standard. Options include Class R fuses (field install Class R Fuse Kit). With Class H or K fuses installed, the switches are UL/CSA listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R fuses (and Class R Fuse Kit installed), the switches are UL/CSA listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.

NOTES:
1) DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability, and will void the warranty.