Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Panel Server support Powerlogic ION Protocol and SY/MAX protocol?

Does the Panel Server support the ION Protocol and SY/MAX protocol, for communication?

Issue
The user needs to know if the Panel Server supports the ION protocol and SY/MAX protocols.

Product Line
Panel Server PAS400 Series, PAS600 Series, and PAS800 Series

Environment
Gateway Protocol Support

Cause
A user needs to convert legacy device protocols such as ION and Powerlogic SY/MAX to Modbus TCP/IP.

Resolution

  • For communication and setup of the new Panel Server:
    • The Panel Server does not support the ION Protocol or Powerlogic SY/MAX protocol.
    • For Powerlogic SY/MAX or ION protocol requirements, there is not a gateway option for these communication protocols.   (The EGX150 is now obsolete)