Issue:
Why does the HDPM6000 have duplicate Modbus registers listed?
Product Line:
HDPM6000
Environment:
HDPM6000 Modbus Register Map
Cause:
The Modbus Register list provides two Modbus registers with the same alarm register with two different Modbus register addresses.
For example: 10220-10227 - Warning and 10820-10831 - Warning.
What is the difference for these two sets of alarm registers?
Resolution
Some registers are legacy and only support up to 120 circuits. (i.e. 10220-10227)
The new registers now support the new features of the HDPM6000 and a total of 192 Circuits. (i.e. 10820-10831)
HDPM6000 Protocol and Modbus Guide: PowerLogic™ HDPM6000 Protocol Guide | Schneider Electric