Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does EXN150T3HB has 220 degree C insulating and does NEC code for insulating system applies on the transformer with 220 degree C insulating temperature rise?

Issue:

Does NEC code for insulating system applies on the transformer with 220 degree C insulating temperature rise?

Does EXN150T3HB has 220 degree C temperature rise?

Product Line:

Low Voltage Transformers

Answer:

The transformer has 220 degree C temperature rise. For the application with NEC code, you will be needing to contact and check this with the local AHJ or local electrical code

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings