Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for the phenolic strips with vertical permanent numbers for the NQ 42 circuit panel?

Issue: Part number for the permanent number strips for the NQ panels

Product Line: Panelboards

Resolution: 80110-190-09 and 80110-190-10 are the left and right 42 circuit strips. Use 21594-12061 screws which they need 6 for one panel.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings