Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the I(n) Specification for Surge Protective Devices?

Issue:

Surge Protective Device Specification

Product Line:

Surge Protective Devices

Environment:

Products sold in North America

Resolution:

Nominal Discharge Currents, often marked as Inominal or I(n) , indicate the amount of current to which sample SPDs have been subject during UL 1449-prescribed tests. Inominal ratings are required to designate the SPD Type, which indicates the environments in which an SPD may be installed. For example, to receive a 20kA Inominal rating, the SPD must survive fifteen 8x20 microsecond transients at 20kA as well as other safety tests.

Schneider Electric Canada
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
  • Register Your Product
  • Blog
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings